BomListDataProviderExportedStatus Enumeration¶
NXOpen.Tooling.BomListDataProvider.ExportedStatus is an alias for NXOpen.Tooling.BomListDataProviderExportedStatus
-
class
NXOpen.Tooling.
BomListDataProviderExportedStatus
¶ Bases:
object
Represents the exported status of a cell.
Enum Members
Enum Member Enum Member Description Null No parts in the row are exported Partial Partial parts in the row are exported All All parts in the row are exported -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-