BomBuilderCircle Enumeration¶
NXOpen.Tooling.BomBuilder.Circle is an alias for NXOpen.Tooling.BomBuilderCircle
-
class
NXOpen.Tooling.
BomBuilderCircle
¶ Bases:
object
Represents an index to the base circle type of cylinder shape.
Enum Members
Enum Member Enum Member Description Circumcircle Circumcircle. InscribedCircle Inscribed circle. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-