BlankNestingBuilderLayoutTypeSpecification Enumeration¶
NXOpen.Tooling.BlankNestingBuilder.LayoutTypeSpecification is an alias for NXOpen.Tooling.BlankNestingBuilderLayoutTypeSpecification
-
class
NXOpen.Tooling.
BlankNestingBuilderLayoutTypeSpecification
¶ Bases:
object
Specifies the layout type of blank nesting.
Enum Members
Enum Member Enum Member Description Rectangle Auto-position blank along x-axis with rectangle bounding box. Parallelogram Auto-position blank along x-axis with parallelogram bounding box. Trapezoid Rotate blank 180 degrees and auto-position it along x-axis with trapezoid bounding box. OneUp Auto-position blank along x-axis without bounding box. TwoUp Two up without bounding box. Move one blank along y-axis, then auto-position them along x-axis. TwoPair Two pair without bounding box. Rotate one blank 180 degrees and move along y-axis, then auto-position them along x-axis. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-