BlankLayoutBuilderLeftRightSideOption Enumeration¶
NXOpen.Tooling.BlankLayoutBuilder.LeftRightSideOption is an alias for NXOpen.Tooling.BlankLayoutBuilderLeftRightSideOption
-
class
NXOpen.Tooling.
BlankLayoutBuilderLeftRightSideOption
¶ Bases:
object
Specifies the option of left right side type.
Enum Members
Enum Member Enum Member Description Average the left right side type of average Left the left side type Right the right side type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-