BendOperationCollection Class¶
-
class
NXOpen.Tooling.
BendOperationCollection
¶ Bases:
object
Creates a
NXOpen.Tooling.BendOperationBuilder
To obtain an instance of this class, refer to
NXOpen.Tooling.ToolingManager
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
CreateBendOperationBuilder | Creates a NXOpen.Tooling.BendOperationBuilder |
FindObject | Finds the NXOpen.Tooling.BendOperationBuilder with the given identifier as recorded in a journal. |
Method Detail¶
CreateBendOperationBuilder¶
-
BendOperationCollection.
CreateBendOperationBuilder
¶ Creates a
NXOpen.Tooling.BendOperationBuilder
Signature
CreateBendOperationBuilder()
Returns: Return type: NXOpen.Tooling.BendOperationBuilder
New in version NX8.5.0.
License requirements: None.
FindObject¶
-
BendOperationCollection.
FindObject
¶ Finds the
NXOpen.Tooling.BendOperationBuilder
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: BendOperationBuilder found Return type: NXOpen.Tooling.BendOperationBuilder
New in version NX8.5.0.
License requirements: None.