BendInsertDesignBuilderBlankPositions Enumeration¶
NXOpen.Tooling.BendInsertDesignBuilder.BlankPositions is an alias for NXOpen.Tooling.BendInsertDesignBuilderBlankPositions
-
class
NXOpen.Tooling.
BendInsertDesignBuilderBlankPositions
¶ Bases:
object
Specifies the blank position.
Enum Members
Enum Member Enum Member Description PunchPlate the blank is on the punch plate StripperPlate the blank is on the stripper plate -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-