BackingPadBuilder Class¶
-
class
NXOpen.Tooling.
BackingPadBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.BackingPadBuilder
which is used to create or delete the Backing Pad.To create a new instance of this class, use
NXOpen.Tooling.ProgressiveDieManager.CreateBackingPadBuilder()
Default values.
Property Value OffsetValueLinearDimension.Value 5 (millimeters part), 0.2 (inches part) OffsetValueLinearDimensionNegativeX.Value 5 (millimeters part), 0.2 (inches part) OffsetValueLinearDimensionNegativeY.Value 5 (millimeters part), 0.2 (inches part) OffsetValueLinearDimensionPositiveX.Value 5 (millimeters part), 0.2 (inches part) OffsetValueLinearDimensionPositiveY.Value 5 (millimeters part), 0.2 (inches part) PadHeightLinearDimension.Value 50 (millimeters part), 2 (inches part) New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
OffsetValueLinearDimension | Returns the offset value linear dimension |
OffsetValueLinearDimensionNegativeX | Returns the offset value linear dimension negative x |
OffsetValueLinearDimensionNegativeY | Returns the offset value linear dimension negative y |
OffsetValueLinearDimensionPositiveX | Returns the offset value linear dimension positive x |
OffsetValueLinearDimensionPositiveY | Returns the offset value linear dimension positive y |
PadBoolean | Returns the pad boolean |
PadHeightLinearDimension | Returns the pad height linear dimension |
PreviousWorkPart | Returns or sets the previous work part |
SelectComponent | Returns the select target component in which to design backing pad |
SelectCurve | Returns the select curve |
SelectFaces | Returns the select faces |
SelectPad | Returns the select backing pad feature to delete |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
DeleteWavedFaces | Delete waved faces to support journamation |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
WaveFaces | Wave selected faces to support journamation |
Enumerations¶
BackingPadBuilderTypes Enumeration | types of backing pad design |
Property Detail¶
OffsetValueLinearDimension¶
-
BackingPadBuilder.
OffsetValueLinearDimension
¶ Returns the offset value linear dimension
-------------------------------------
Getter Method
Signature
OffsetValueLinearDimension
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
OffsetValueLinearDimensionNegativeX¶
-
BackingPadBuilder.
OffsetValueLinearDimensionNegativeX
¶ Returns the offset value linear dimension negative x
-------------------------------------
Getter Method
Signature
OffsetValueLinearDimensionNegativeX
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
OffsetValueLinearDimensionNegativeY¶
-
BackingPadBuilder.
OffsetValueLinearDimensionNegativeY
¶ Returns the offset value linear dimension negative y
-------------------------------------
Getter Method
Signature
OffsetValueLinearDimensionNegativeY
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
OffsetValueLinearDimensionPositiveX¶
-
BackingPadBuilder.
OffsetValueLinearDimensionPositiveX
¶ Returns the offset value linear dimension positive x
-------------------------------------
Getter Method
Signature
OffsetValueLinearDimensionPositiveX
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
OffsetValueLinearDimensionPositiveY¶
-
BackingPadBuilder.
OffsetValueLinearDimensionPositiveY
¶ Returns the offset value linear dimension positive y
-------------------------------------
Getter Method
Signature
OffsetValueLinearDimensionPositiveY
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
PadBoolean¶
-
BackingPadBuilder.
PadBoolean
¶ Returns the pad boolean
-------------------------------------
Getter Method
Signature
PadBoolean
Returns: Return type: NXOpen.GeometricUtilities.BooleanOperation
New in version NX10.0.0.
License requirements: None.
PadHeightLinearDimension¶
-
BackingPadBuilder.
PadHeightLinearDimension
¶ Returns the pad height linear dimension
-------------------------------------
Getter Method
Signature
PadHeightLinearDimension
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
PreviousWorkPart¶
-
BackingPadBuilder.
PreviousWorkPart
¶ Returns or sets the previous work part
-------------------------------------
Getter Method
Signature
PreviousWorkPart
Returns: Return type: NXOpen.Part
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PreviousWorkPart
Parameters: previousWorkPart ( NXOpen.Part
) –New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
SelectComponent¶
-
BackingPadBuilder.
SelectComponent
¶ Returns the select target component in which to design backing pad
-------------------------------------
Getter Method
Signature
SelectComponent
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX10.0.0.
License requirements: None.
SelectCurve¶
-
BackingPadBuilder.
SelectCurve
¶ Returns the select curve
-------------------------------------
Getter Method
Signature
SelectCurve
Returns: Return type: NXOpen.Section
New in version NX10.0.0.
License requirements: None.
SelectFaces¶
-
BackingPadBuilder.
SelectFaces
¶ Returns the select faces
-------------------------------------
Getter Method
Signature
SelectFaces
Returns: Return type: NXOpen.SelectFaceList
New in version NX10.0.0.
License requirements: None.
SelectPad¶
-
BackingPadBuilder.
SelectPad
¶ Returns the select backing pad feature to delete
-------------------------------------
Getter Method
Signature
SelectPad
Returns: Return type: NXOpen.Features.SelectFeatureList
New in version NX10.0.0.
License requirements: None.
Type¶
-
BackingPadBuilder.
Type
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Tooling.BackingPadBuilderTypes
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Tooling.BackingPadBuilderTypes
) –New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
DeleteWavedFaces¶
-
BackingPadBuilder.
DeleteWavedFaces
¶ Delete waved faces to support journamation
Signature
DeleteWavedFaces()
New in version NX10.0.0.
License requirements: None.
Validate¶
-
BackingPadBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.