AutoDimensionBuilderValuePrecisionType Enumeration

NXOpen.Tooling.AutoDimensionBuilder.ValuePrecisionType is an alias for NXOpen.Tooling.AutoDimensionBuilderValuePrecisionType

class NXOpen.Tooling.AutoDimensionBuilderValuePrecisionType

Bases: object

value precision type

Enum Members

Enum Member Enum Member Description
NominalMinusX
NominalMinusXDotx
NominalMinusXDotxx
NominalMinusXDotxxx
NominalMinusXDotxxxx
NominalMinusXDotxxxxx
NominalMinusXDotxxxxxx
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.