AutoDimensionBuilderTextOrientationType Enumeration

NXOpen.Tooling.AutoDimensionBuilder.TextOrientationType is an alias for NXOpen.Tooling.AutoDimensionBuilderTextOrientationType

class NXOpen.Tooling.AutoDimensionBuilderTextOrientationType

Bases: object

text orientation type

Enum Members

Enum Member Enum Member Description
Horizontal
Aligned
TextOverDimensionLine
TextAtAngle
Perpendicular
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.