AutoDimensionBuilderMainType Enumeration

NXOpen.Tooling.AutoDimensionBuilder.MainType is an alias for NXOpen.Tooling.AutoDimensionBuilderMainType

class NXOpen.Tooling.AutoDimensionBuilderMainType

Bases: object

create or edit ordinate dimension

Enum Members

Enum Member Enum Member Description
CreateOrdinateDimension
EditOrdinateDimension
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.