AssignPatchBuilderConvertTypeOption Enumeration¶
NXOpen.Tooling.AssignPatchBuilder.ConvertTypeOption is an alias for NXOpen.Tooling.AssignPatchBuilderConvertTypeOption
-
class
NXOpen.Tooling.
AssignPatchBuilderConvertTypeOption
¶ Bases:
object
The option to convert to have copies or no copies for all selected sheets.
Enum Members
Enum Member Enum Member Description WithCopies NoCopies -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-