AssemblyDrawingBuilderViewOptionValue Enumeration

NXOpen.Tooling.AssemblyDrawingBuilder.ViewOptionValue is an alias for NXOpen.Tooling.AssemblyDrawingBuilderViewOptionValue

class NXOpen.Tooling.AssemblyDrawingBuilderViewOptionValue

Bases: object

Specifies the view options.

Enum Members

Enum Member Enum Member Description
DefaultView
BaseViewTool
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.