AssemblyDrawingBuilderModelViewToUseValue Enumeration

NXOpen.Tooling.AssemblyDrawingBuilder.ModelViewToUseValue is an alias for NXOpen.Tooling.AssemblyDrawingBuilderModelViewToUseValue

class NXOpen.Tooling.AssemblyDrawingBuilderModelViewToUseValue

Bases: object

Specifies the model view to use.

Enum Members

Enum Member Enum Member Description
Top
Front
Right
Back
Bottom
Left
Isometric
Trimetric
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.