AssemblyDrawingBuilderDrawingTypes Enumeration

NXOpen.Tooling.AssemblyDrawingBuilder.DrawingTypes is an alias for NXOpen.Tooling.AssemblyDrawingBuilderDrawingTypes

class NXOpen.Tooling.AssemblyDrawingBuilderDrawingTypes

Bases: object

Specifies the drawing type.

Enum Members

Enum Member Enum Member Description
MasterModel
SelfContained
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.