AssemblyDrawingBuilderDrawingCreateOrEdit Enumeration

NXOpen.Tooling.AssemblyDrawingBuilder.DrawingCreateOrEdit is an alias for NXOpen.Tooling.AssemblyDrawingBuilderDrawingCreateOrEdit

class NXOpen.Tooling.AssemblyDrawingBuilderDrawingCreateOrEdit

Bases: object

Specifies the sheet operation.

Enum Members

Enum Member Enum Member Description
CreateNew
Sh1
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.