AssemblyDrawingBuilderAttributeNames Enumeration

NXOpen.Tooling.AssemblyDrawingBuilder.AttributeNames is an alias for NXOpen.Tooling.AssemblyDrawingBuilderAttributeNames

class NXOpen.Tooling.AssemblyDrawingBuilderAttributeNames

Bases: object

Specifies the attribute name

Enum Members

Enum Member Enum Member Description
MwSide
MwComponentName
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.