AddReusablePartPocketBodyMethod Enumeration¶
NXOpen.Tooling.AddReusablePart.PocketBodyMethod is an alias for NXOpen.Tooling.AddReusablePartPocketBodyMethod
-
class
NXOpen.Tooling.
AddReusablePartPocketBodyMethod
¶ Bases:
object
Represents save pocket body information, updating or deleting a pocket body size mode method
Enum Members
Enum Member Enum Member Description NotSet Save pocket body information into attatched component Update Update the existed pocket body size Delete Delete pocket body -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-