TextColorFontWidthBuilder Class¶
-
class
NXOpen.
TextColorFontWidthBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represent a
NXOpen.TextColorFontWidthBuilder
This is a sub-builder class and cannot be directly instantiated
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
TextColor | Returns or sets the text color |
TextFont | Returns or sets the text font |
TextStyle | Returns or sets the text style |
TextWidth | Returns or sets the text width |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
TextColor¶
-
TextColorFontWidthBuilder.
TextColor
¶ Returns or sets the text color
-------------------------------------
Getter Method
Signature
TextColor
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TextColor
Parameters: textColor (Id) – New in version NX9.0.0.
License requirements: None.
TextFont¶
-
TextColorFontWidthBuilder.
TextFont
¶ Returns or sets the text font
-------------------------------------
Getter Method
Signature
TextFont
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TextFont
Parameters: textFont (str) – New in version NX9.0.0.
License requirements: None.
TextStyle¶
-
TextColorFontWidthBuilder.
TextStyle
¶ Returns or sets the text style
-------------------------------------
Getter Method
Signature
TextStyle
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TextStyle
Parameters: textStyle (str) – New in version NX9.0.0.
License requirements: None.
TextWidth¶
-
TextColorFontWidthBuilder.
TextWidth
¶ Returns or sets the text width
-------------------------------------
Getter Method
Signature
TextWidth
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TextWidth
Parameters: textWidth (str) – New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
TextColorFontWidthBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.