SketchViewReorient Enumeration¶
NXOpen.Sketch.ViewReorient is an alias for NXOpen.SketchViewReorient
-
class
NXOpen.
SketchViewReorient
¶ Bases:
object
Used to indicate whether to reorient the view when the sketch is activated
Enum Members
Enum Member Enum Member Description False Do not reorient view to sketch True Reorient view to sketch -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-