SketchUpdateLevel Enumeration¶
NXOpen.Sketch.UpdateLevel is an alias for NXOpen.SketchUpdateLevel
-
class
NXOpen.
SketchUpdateLevel
¶ Bases:
object
Used to indicate how much the updating should occur
Enum Members
Enum Member Enum Member Description SketchOnly Only update the sketch Model Update the full model and the sketch -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-