SketchDimensionOption Enumeration¶
NXOpen.Sketch.DimensionOption is an alias for NXOpen.SketchDimensionOption
-
class
NXOpen.
SketchDimensionOption
¶ Bases:
object
Used by
NXOpen.Sketch.CreateDimension()
,NXOpen.Sketch.CreateRadialDimension()
NXOpen.Sketch.CreateDiameterDimension()
andNXOpen.Sketch.CreatePerimeterDimension()
to determine whether to create driving or reference dimensionEnum Members
Enum Member Enum Member Description CreateAsDriving Create dimension as driving CreateAsReference Create dimension as reference CreateAsAutomatic Create dimension as automatic -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-