SketchDimensionBuilderExpOption Enumeration¶
NXOpen.SketchDimensionBuilder.ExpOption is an alias for NXOpen.SketchDimensionBuilderExpOption
-
class
NXOpen.
SketchDimensionBuilderExpOption
¶ Bases:
object
This enum determines the expression behavior when a dimension is attached to new geometry
Enum Members
Enum Member Enum Member Description KeepExpression keep expression, adjust geometry MeasureGeometry remove expression, measure geometry -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-