SketchConstraintType Enumeration¶
NXOpen.Sketch.ConstraintType is an alias for NXOpen.SketchConstraintType
-
class
NXOpen.
SketchConstraintType
¶ Bases:
object
Represents the type of constraint
Enum Members
Enum Member Enum Member Description NoCon Used in query methods that filter by constraint type to select any type of constraint Fixed Horizontal Vertical Parallel Perpendicular Collinear EqualLength EqualRadius ConstantLength ConstantAngle Coincident Concentric Mirror PointOnCurve Midpoint Tangent RadiusDim DiameterDim HorizontalDim VerticalDim ParallelDim PerpendicularDim AngularDim system will decide if it is major or minor ReservedCon1 Do not use ReservedCon2 Do not use ReservedCon3 Do not use ReservedCon4 Do not use ReservedCon5 Do not use ReservedCon6 Do not use PointOnString Slope UniformScaled NonUniformScaled AssocTrim Limited support AssocOffset Limited support PerimeterDim Offset Normal PointOnLoop RecipeTrim Pattern MinorAngularDim MajorAngularDim LastConType The last constraint type indicator; NOT to be used. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-