SketchConstraintGeometryHelp_Struct Struct¶
NXOpen.Sketch.ConstraintGeometryHelp is an alias for NXOpen.SketchConstraintGeometryHelp_Struct
-
class
NXOpen.
SketchConstraintGeometryHelp_Struct
¶ Bases:
object
Used by several constraint creation methods that need a help point or parameter to indicate how to create the constraint.
The manner that the help point is used depends on the type of constraint . Constructor: NXOpen.Sketch.ConstraintGeometryHelp()
Fields¶
Field | Description |
---|---|
Type | Point or Parameter |
Point | Ignored unless type is Point |
Parameter | Ignored unless type is Parameter. |
Type¶
-
SketchConstraintGeometryHelp_Struct.
Type
¶ Point or Parameter
-------------------------------------
Field Value Type:
NXOpen.SketchConstraintGeometryHelpType
Point¶
-
SketchConstraintGeometryHelp_Struct.
Point
¶ Ignored unless type is Point
-------------------------------------
Field Value Type:
NXOpen.Point3d