SketchConstraintClass Enumeration¶
NXOpen.Sketch.ConstraintClass is an alias for NXOpen.SketchConstraintClass
-
class
NXOpen.
SketchConstraintClass
¶ Bases:
object
Represents the class of the constraint. There are two classes of constraints: geometric and dimension
Enum Members
Enum Member Enum Member Description NotConstraint Any Used in query methods that filter by constraint class to select both types of constraints Geometric A non-dimension constraint Dimension A dimensional constraint -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-