SketchChamferBuilderChamferOptions Enumeration¶
NXOpen.SketchChamferBuilder.ChamferOptions is an alias for NXOpen.SketchChamferBuilderChamferOptions
-
class
NXOpen.
SketchChamferBuilderChamferOptions
¶ Bases:
object
Dialog options for Chamfer Creation
Enum Members
Enum Member Enum Member Description Symmetric Symmetric - specify one distance Asymmetric Asymmetric - specify two distances OffsetandAngle OffsetandAngle - specify offset distance and angle -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-