NXOpen.SheetMetal Package¶
Classes¶
FlatPatternSettings Class | Provides access to object and callout properties for sheet-metal data in flat pattern views on drawings. |
SheetMetalFeatureCollectionValidator Class | SheetMetalFeatureCollectionValidator |
Enumerations¶
FlatPatternSettingsFlatPatternObjectType Enumeration | The members of the following enumerated type are used to identify object types to the FlatPatternView API. |
Structs¶
FlatPatternSettingsFlatPatternCalloutTypeDisplay_Struct Struct | The members of the following structure are the display data for a callout in a flat pattern drawing member view. |
FlatPatternSettingsFlatPatternObjectTypeDisplay_Struct Struct | The members of the following structure are the display data for an object in a flat pattern drawing member view. |