SessionProjectAssignmentState Enumeration¶
NXOpen.Session.ProjectAssignmentState is an alias for NXOpen.SessionProjectAssignmentState
-
class
NXOpen.
SessionProjectAssignmentState
¶ Bases:
object
Indicates project assignment state
Enum Members
Enum Member Enum Member Description NotSet to remove project from all objects Partial to skip project assignment Full to assign project to all objects -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-