SelectionUistylerSelectionType Enumeration¶
NXOpen.Selection.UistylerSelectionType is an alias for NXOpen.SelectionUistylerSelectionType
-
class
NXOpen.
SelectionUistylerSelectionType
¶ Bases:
object
Indicates the general class of object to filter selection.
Enum Members
Enum Member Enum Member Description InactiveSelection sets selection inactive until this function is called again SingleSelection allows single select SingleDeselection single deselect RobustSelection reselect last SinglePosition the position is returned if no object is selected with the single select gesture RectanglePosition the position is returned if no object is selected with the single select gesture -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-