SelectionSelectionType Enumeration¶
NXOpen.Selection.SelectionType is an alias for NXOpen.SelectionSelectionType
-
class
NXOpen.
SelectionSelectionType
¶ Bases:
object
Indicates the general class of object to filter selection.
Enum Members
Enum Member Enum Member Description All Filter to select all object types Features Filter to select all feature types Curves Filter to select all curve types Faces Filter to select all face types Edges Filter to select all edge types CurvesAndEdges Filter to select all curve and edge types -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-