SelectionSelectionDescriptor_Struct Struct¶
NXOpen.Selection.SelectionDescriptor is an alias for NXOpen.SelectionSelectionDescriptor_Struct
-
class
NXOpen.
SelectionSelectionDescriptor_Struct
¶ Bases:
object
For a rectangle deselection, the fields ** Deselection **, ** MultipleSelection **, ** Rectangle ** bits would be set.
For a name selection which selected one object, the fields ** SelectionDescriptor.Selection **, ** SingleSelection **, and ** NameSelection ** bits would be set. If a reselect was done (an object is selected and the previous object selected is deselected), only the field ** SelectionDescriptor.Reselection ** bit is set. The fields ** SingleSelection ** and ** MultipleSelection ** bits are not set for position. The field ** Rectangle ** bit is set for rectangle selection, rectangle deselection, and rectangle position. This function can be used with UIStyler dialogs and can be called from either the selection filter procedure or the selection callback. . Constructor: NXOpen.Selection.SelectionDescriptor()
Fields¶
Field | Description |
---|---|
Selection | |
Deselection | |
Reselection | |
SingleSelection | |
MultipleSelection | |
SinglePosition | |
RectanglePosition | |
NameSelection | |
Rectangle |
Selection¶
-
SelectionSelectionDescriptor_Struct.
Selection
¶ -------------------------------------
Field Value Type:bool
Deselection¶
-
SelectionSelectionDescriptor_Struct.
Deselection
¶ -------------------------------------
Field Value Type:bool
Reselection¶
-
SelectionSelectionDescriptor_Struct.
Reselection
¶ -------------------------------------
Field Value Type:bool
SingleSelection¶
-
SelectionSelectionDescriptor_Struct.
SingleSelection
¶ -------------------------------------
Field Value Type:bool
MultipleSelection¶
-
SelectionSelectionDescriptor_Struct.
MultipleSelection
¶ -------------------------------------
Field Value Type:bool
SinglePosition¶
-
SelectionSelectionDescriptor_Struct.
SinglePosition
¶ -------------------------------------
Field Value Type:bool
RectanglePosition¶
-
SelectionSelectionDescriptor_Struct.
RectanglePosition
¶ -------------------------------------
Field Value Type:bool