SectionDeselectOption Enumeration¶
NXOpen.Section.DeselectOption is an alias for NXOpen.SectionDeselectOption
-
class
NXOpen.
SectionDeselectOption
¶ Bases:
object
Defines type of deselect option.
Enum Members
Enum Member Enum Member Description SectionBetweenIntersection Potion of the loop between intersections will be deselected this may contain multiple chains CurveBetweenIntersection Portion of curve between intersection -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-