SectionCollectionLoopOption Enumeration¶
NXOpen.SectionCollection.LoopOption is an alias for NXOpen.SectionCollectionLoopOption
-
class
NXOpen.
SectionCollectionLoopOption
¶ Bases:
object
Defines how section are created in
SectionCollection.CreateSectionsUsingCurves()
Enum Members
Enum Member Enum Member Description Separate One section is created for each loop SeparateOuter One section per outer loop and enclosed inner loops -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-