SectionAllowTypes Enumeration¶
NXOpen.Section.AllowTypes is an alias for NXOpen.SectionAllowTypes
-
class
NXOpen.
SectionAllowTypes
¶ Bases:
object
Defines entity types allowed.
Enum Members
Enum Member Enum Member Description Uninitialized This is uninitialized state. Do not use this. OnlyCurves Allow only curves in section OnlyPoints Allow only points in section CurvesAndPoints Allow both points and curves in section -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-