ScalarTableValue Class¶
-
class
NXOpen.
ScalarTableValue
¶ Bases:
NXOpen.GeneralScalarTable
Represents a General M x N table of scalar (real) values.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
NumCols | Returns the numuber of columns |
NumRows | Returns the number of rows |
Methods¶
Method | Description |
---|---|
Dispose | Destroys the object |
GetCellValue | Returns the cell value |
GetNthColumn | Returns the entire Nth column of values. |
GetNthColumnUnits | Returns the entire Nth column of values. |
GetNthRow | Returns the entire Nth row of values. |
SetCellNoValue | Sets cell as having no value |
SetCellValue | Sets cell value |
SetNthColumn | Sets the entire Nth column of values. |
SetNthColumnUnits | Sets the entire Nth column of values. |
SetNthRow | Sets the entire Nth row of values. |
SetNumberOfRows | Sets the number of rows |
SetTableSize | Sets the table size |