SinumerikCaSimplifyBodiesBuilderObjectToReplaceWithTypes Enumeration¶
NXOpen.SIM.SinumerikCaSimplifyBodiesBuilder.ObjectToReplaceWithTypes is an alias for NXOpen.SIM.SinumerikCaSimplifyBodiesBuilderObjectToReplaceWithTypes
-
class
NXOpen.SIM.
SinumerikCaSimplifyBodiesBuilderObjectToReplaceWithTypes
¶ Bases:
object
The object to replaces with types
Enum Members
Enum Member Enum Member Description Nothing Nothing ConvexHull Convex Hull BoundingSphere Bounding Sphere BoundingBlock Bounding Block BoundingCylinder Bounding Cylinder InscribedCylinder Inscribed Cylinder -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-