SimDebugBuilderUiType Enumeration¶
NXOpen.SIM.SimDebugBuilder.UiType is an alias for NXOpen.SIM.SimDebugBuilderUiType
-
class
NXOpen.SIM.
SimDebugBuilderUiType
¶ Bases:
object
Represents the ui type
Enum Members
Enum Member Enum Member Description DisplayMomEvent Display Mom Event ShowPartAndTipJunctions Show Part And Tip Junction GenerateSpinningTools Generate Spinning Tools UseHybridGougeChecker Use Hybrid Gouge Checker UseMtbOldDialogs Use MTB Old Dialogs UseFastTicker Use Fast Ticker PrintOutTraceSerialNumbers Print Out Trace Serial Numbers PerformanceDisplayDetail Performance Display Detail PerformanceDisplayTime Performance Display Time PerformanceIndentTime Performance Indent Time PerformanceDisplayData Performance Display Data DctkWriteCollisionPairs Write Collision Pairs -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-