SimDebugBuilderTraceType Enumeration¶
NXOpen.SIM.SimDebugBuilder.TraceType is an alias for NXOpen.SIM.SimDebugBuilderTraceType
-
class
NXOpen.SIM.
SimDebugBuilderTraceType
¶ Bases:
object
Represents the trace type
Enum Members
Enum Member Enum Member Description ButtonDown Trace Button Down Vcr Trace Vcr Ipw Trace Ipw Performance Trace Performance Collision Trace Collision Gouge Trace Gouge Highlighting Trace Highlighting Details Trace Details PositionalIsv Trace Positional Isv SpinningNonSpinning Trace Spinning Nonspinning KinematicModel Trace Kinematic Model Event Trace Event LineServer Trace Line Server Sync Trace Sync DctkSettings Trace Dctk Settings DctkMovements Trace Dctk Movements DctkDisplay Trace Dctk Display DctkCollision Trace Dctk Collision ToolPathPicking Trace ToolPath Picking -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-