SimDebugBuilderOutputType Enumeration¶
NXOpen.SIM.SimDebugBuilder.OutputType is an alias for NXOpen.SIM.SimDebugBuilderOutputType
-
class
NXOpen.SIM.
SimDebugBuilderOutputType
¶ Bases:
object
The output type
Enum Members
Enum Member Enum Member Description Syslog Output to syslog ListingWindow Output to listing window Autotest Output to autotest ToFile Output to file -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-