SimDebugBuilderDumpType Enumeration¶
NXOpen.SIM.SimDebugBuilder.DumpType is an alias for NXOpen.SIM.SimDebugBuilderDumpType
-
class
NXOpen.SIM.
SimDebugBuilderDumpType
¶ Bases:
object
Represents the dump type
Enum Members
Enum Member Enum Member Description NotSet Dump Nothing KinematicModel Dump Kinematic Model Highlighting Dump Highlighting Ipw Dump IPW Collision Dump Collision OutputBuffer Dump Output Buffer Time Dump Time Details Dump Details SynchronizeUi Dump Synchronize UI SynchronizeManagerXtp Dump SynchronizeManagerXtp EngineParams Dump Engine Params MomVariables Dump Mom Variables DebugUi Dump Debug UI SimulationSettings Dump Simulation Settings SimManager Dump SimManager PathEvents Dump Path Events MachiningTimeAnalysis Dump Machining Time Analysis -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-