MachineToolConfigurationTechnologyTypes Enumeration¶
NXOpen.SIM.MachineToolConfiguration.TechnologyTypes is an alias for NXOpen.SIM.MachineToolConfigurationTechnologyTypes
-
class
NXOpen.SIM.
MachineToolConfigurationTechnologyTypes
¶ Bases:
object
The machine technology types
Enum Members
Enum Member Enum Member Description Mill The mill technology type Turn The lathe technology type Millturn The millturn technology type NotSet No technology type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-