MachineToolConfigurationSwivelingTypes Enumeration¶
NXOpen.SIM.MachineToolConfiguration.SwivelingTypes is an alias for NXOpen.SIM.MachineToolConfigurationSwivelingTypes
-
class
NXOpen.SIM.
MachineToolConfigurationSwivelingTypes
¶ Bases:
object
The machine swiveling types
Enum Members
Enum Member Enum Member Description Cycle800 The CYCLE800 swiveling type Transarot The TRANS/AROT swiveling type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-