MachineToolConfigurationPlaneTypes Enumeration¶
NXOpen.SIM.MachineToolConfiguration.PlaneTypes is an alias for NXOpen.SIM.MachineToolConfigurationPlaneTypes
-
class
NXOpen.SIM.
MachineToolConfigurationPlaneTypes
¶ Bases:
object
The plane selection types
Enum Members
Enum Member Enum Member Description Operator The operator panel plane type G17 The G17 plane type G18 The G18 plane type G19 The G19 plane type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-