MachineKitBuilder Class¶
-
class
NXOpen.SIM.
MachineKitBuilder
¶ Bases:
NXOpen.Builder
This class is used for the Machine Kit Create Dialog.
Calling
Builder.Commit()
on this builder will start the machine kit creation process and return None.Use the
Part
class to create a MachineKitBuilder object.New in version NX10.0.2.
Properties¶
Property | Description |
---|---|
Name | Returns or sets the machine kit name. |
OutputDirectory | Returns or sets the machine kit output directory. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Name¶
-
MachineKitBuilder.
Name
¶ Returns or sets the machine kit name.
The name is used for the database entry and the name of the folder.
-------------------------------------
Getter Method
Signature
Name
Returns: machine kit name Return type: str New in version NX10.0.2.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
Name
Parameters: kitName (str) – machine kit name New in version NX10.0.2.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
OutputDirectory¶
-
MachineKitBuilder.
OutputDirectory
¶ Returns or sets the machine kit output directory.
This is the location of the machine folder.
-------------------------------------
Getter Method
Signature
OutputDirectory
Returns: machine kit output directory Return type: str New in version NX10.0.2.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
OutputDirectory
Parameters: outputDirectory (str) – machine kit output directory New in version NX10.0.2.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
Method Detail¶
Validate¶
-
MachineKitBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.