KinematicComponentBuilderSystemClass Enumeration¶
NXOpen.SIM.KinematicComponentBuilder.SystemClass is an alias for NXOpen.SIM.KinematicComponentBuilderSystemClass
-
class
NXOpen.SIM.
KinematicComponentBuilderSystemClass
¶ Bases:
object
The SIM KIM system classes
Enum Members
Enum Member Enum Member Description Machine Machine Base classification Tool Tool classification Turret Device classification Pocket Static Holder classification Temporary Temporary classification Part Part - Setup classification Workpiece Workpiece - Setup classification SetupElement Any setup element classification Basic On available in a BASIC machine. If this bit is set, then the machine part can be used for simulation when only UG_ISV_BASIC license is available LatheSpindle Lathe Spindle classification PocketOnHead Dynamic Holder classification ToolCutting Tool Cutting classification Spinning Spinning classification Head Head class ToolNonCutting -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-