KinematicComponentBuilderRegisterTypes Enumeration¶
NXOpen.SIM.KinematicComponentBuilder.RegisterTypes is an alias for NXOpen.SIM.KinematicComponentBuilderRegisterTypes
-
class
NXOpen.SIM.
KinematicComponentBuilderRegisterTypes
¶ Bases:
object
The register types
Enum Members
Enum Member Enum Member Description SameAsPocketId the pocket id defined the register Specify the register is specified -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-