IsvControlPanelBuilderVncMode Enumeration¶
NXOpen.SIM.IsvControlPanelBuilder.VncMode is an alias for NXOpen.SIM.IsvControlPanelBuilderVncMode
-
class
NXOpen.SIM.
IsvControlPanelBuilderVncMode
¶ Bases:
object
Type of VNC Mode
Enum Members
Enum Member Enum Member Description Error ERROR Notconnected NOT CONNECTED Connected CONNECTED Booted BOOTED Configured CONFIGURED Initialized INITIALIZED ProgramsLoaded PROGRAMS LOADED Reset RESET Stop STOP Start START Run RUN -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-