IsvControlPanelBuilderVisualizationType Enumeration¶
NXOpen.SIM.IsvControlPanelBuilder.VisualizationType is an alias for NXOpen.SIM.IsvControlPanelBuilderVisualizationType
-
class
NXOpen.SIM.
IsvControlPanelBuilderVisualizationType
¶ Bases:
object
The Visualization type
Enum Members
Enum Member Enum Member Description MachineCodeSimulateCse Machine Code Simulate Cse MachineCodeSimulateMtd Machine Code Simulate Mtd ToolPathSimulation Tool Path Simulate -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-