RuleManagerInitializationStatusType Enumeration¶
NXOpen.RuleManager.InitializationStatusType is an alias for NXOpen.RuleManagerInitializationStatusType
-
class
NXOpen.
RuleManagerInitializationStatusType
¶ Bases:
object
Indicates the status from initializing RuleManager.
Enum Members
Enum Member Enum Member Description Success Initialization succeeded Failure Initialization failed Unavailable Intent not available UnableToObtainLicense Cannot obtain license CloseFailure Close failed -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-