RuleManagerFilter Enumeration¶
NXOpen.RuleManager.Filter is an alias for NXOpen.RuleManagerFilter
-
class
NXOpen.
RuleManagerFilter
¶ Bases:
object
The filter option for asking for classes.
Enum Members
Enum Member Enum Member Description User User classes only System System classes only Both Both user and system classes UserPlus User and application classes UserLoaded User classes that are loaded SystemLoaded System classes that are loaded BothLoaded System and user classes that are loaded UserPlusLoaded User and application classes that are loaded -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-